InspectionLimitsOfSizeModeBuilder Class¶
-
class
NXOpen.CAM.
InspectionLimitsOfSizeModeBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable limits of size mode enum value
New in version NX8.5.1.
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current limits of size mode |
Methods¶
Property Detail¶
Value¶
-
InspectionLimitsOfSizeModeBuilder.
Value
¶ Returns or sets the current limits of size mode
-------------------------------------
Getter Method
Signature
Value()
Returns: the current limits of size mode Return type: NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value(itemValue)
Parameters: itemValue ( NXOpen.CAM.InspectionMethodBuilderLimitsOfSizeTypes
) – the new limits of size modeNew in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)