InspectionEdgePointFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionEdgePointFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Edge Point Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionEdgePointFeatureBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CsysReferenceType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the name of the inspection edge point feature |
NormalVectorI | Returns or sets the point normal vector I component |
NormalVectorJ | Returns or sets the point normal vector J component |
NormalVectorK | Returns or sets the point normal vector K component |
Notes | Returns the notes builder |
OffsetValue | Returns the point offset value |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PointX | Returns or sets the point X coordinate |
PointY | Returns or sets the point Y coordinate |
PointZ | Returns or sets the point Z coordinate |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseEdgeDirection | Returns or sets the reverse point normal direction |
ReverseSurfaceDirection | Returns or sets the reverse surface normal direction |
SafeClearance | Returns the safe clearance builder |
SelectAdjacentSurface | Returns the select adjacent surface |
SelectPoint | Returns or sets the selected edge point |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
SurfaceNormalVectorI | Returns or sets the surface normal vector I component |
SurfaceNormalVectorJ | Returns or sets the surface normal vector J component |
SurfaceNormalVectorK | Returns or sets the surface normal vector K component |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipNormal | Flips the edge point inspection feature normal vector |
FlipSurfaceNormal | Flips the edge point inspection feature adjacent surface normal vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetAdjacentSurface | Sets the edge point inspection feature adjacent surface tag |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateOffset | Updates the edge point inspection feature when the offset value is changed |
UpdateParams | Updates edge point inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CsysReferenceType¶
-
InspectionEdgePointFeatureBuilder.
CsysReferenceType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysReferenceType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysReferenceType(csysReferenceType)
Parameters: csysReferenceType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionEdgePointFeatureBuilder.
Name
¶ Returns or sets the name of the inspection edge point feature
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorI¶
-
InspectionEdgePointFeatureBuilder.
NormalVectorI
¶ Returns or sets the point normal vector I component
-------------------------------------
Getter Method
Signature
NormalVectorI()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorI(normalVectorI)
Parameters: normalVectorI (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorJ¶
-
InspectionEdgePointFeatureBuilder.
NormalVectorJ
¶ Returns or sets the point normal vector J component
-------------------------------------
Getter Method
Signature
NormalVectorJ()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorJ(normalVectorJ)
Parameters: normalVectorJ (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorK¶
-
InspectionEdgePointFeatureBuilder.
NormalVectorK
¶ Returns or sets the point normal vector K component
-------------------------------------
Getter Method
Signature
NormalVectorK()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorK(normalVectorK)
Parameters: normalVectorK (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetValue¶
-
InspectionEdgePointFeatureBuilder.
OffsetValue
¶ Returns the point offset value
-------------------------------------
Getter Method
Signature
OffsetValue()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
PointX¶
-
InspectionEdgePointFeatureBuilder.
PointX
¶ Returns or sets the point X coordinate
-------------------------------------
Getter Method
Signature
PointX()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointX(pointX)
Parameters: pointX (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointY¶
-
InspectionEdgePointFeatureBuilder.
PointY
¶ Returns or sets the point Y coordinate
-------------------------------------
Getter Method
Signature
PointY()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointY(pointY)
Parameters: pointY (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointZ¶
-
InspectionEdgePointFeatureBuilder.
PointZ
¶ Returns or sets the point Z coordinate
-------------------------------------
Getter Method
Signature
PointZ()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointZ(pointZ)
Parameters: pointZ (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseEdgeDirection¶
-
InspectionEdgePointFeatureBuilder.
ReverseEdgeDirection
¶ Returns or sets the reverse point normal direction
-------------------------------------
Getter Method
Signature
ReverseEdgeDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseEdgeDirection(reverseEdgeDirection)
Parameters: reverseEdgeDirection (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseSurfaceDirection¶
-
InspectionEdgePointFeatureBuilder.
ReverseSurfaceDirection
¶ Returns or sets the reverse surface normal direction
-------------------------------------
Getter Method
Signature
ReverseSurfaceDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseSurfaceDirection(reverseSurfaceDirection)
Parameters: reverseSurfaceDirection (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectAdjacentSurface¶
-
InspectionEdgePointFeatureBuilder.
SelectAdjacentSurface
¶ Returns the select adjacent surface
-------------------------------------
Getter Method
Signature
SelectAdjacentSurface()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
SelectPoint¶
-
InspectionEdgePointFeatureBuilder.
SelectPoint
¶ Returns or sets the selected edge point
-------------------------------------
Getter Method
Signature
SelectPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectPoint(selectPoint)
Parameters: selectPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceNormalVectorI¶
-
InspectionEdgePointFeatureBuilder.
SurfaceNormalVectorI
¶ Returns or sets the surface normal vector I component
-------------------------------------
Getter Method
Signature
SurfaceNormalVectorI()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceNormalVectorI(surfaceNormalVectorI)
Parameters: surfaceNormalVectorI (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceNormalVectorJ¶
-
InspectionEdgePointFeatureBuilder.
SurfaceNormalVectorJ
¶ Returns or sets the surface normal vector J component
-------------------------------------
Getter Method
Signature
SurfaceNormalVectorJ()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceNormalVectorJ(surfaceNormalVectorJ)
Parameters: surfaceNormalVectorJ (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SurfaceNormalVectorK¶
-
InspectionEdgePointFeatureBuilder.
SurfaceNormalVectorK
¶ Returns or sets the surface normal vector K component
-------------------------------------
Getter Method
Signature
SurfaceNormalVectorK()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SurfaceNormalVectorK(surfaceNormalVectorK)
Parameters: surfaceNormalVectorK (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
FlipNormal¶
-
InspectionEdgePointFeatureBuilder.
FlipNormal
¶ Flips the edge point inspection feature normal vector
Signature
FlipNormal()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FlipSurfaceNormal¶
-
InspectionEdgePointFeatureBuilder.
FlipSurfaceNormal
¶ Flips the edge point inspection feature adjacent surface normal vector
Signature
FlipSurfaceNormal()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetAdjacentSurface¶
-
InspectionEdgePointFeatureBuilder.
SetAdjacentSurface
¶ Sets the edge point inspection feature adjacent surface tag
Signature
SetAdjacentSurface(adjacentSurface)
Parameters: adjacentSurface ( NXOpen.Face
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateOffset¶
-
InspectionEdgePointFeatureBuilder.
UpdateOffset
¶ Updates the edge point inspection feature when the offset value is changed
Signature
UpdateOffset()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionEdgePointFeatureBuilder.
UpdateParams
¶ Updates edge point inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionEdgePointFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.