InspectionDeltaMoveBuilder Class¶
-
class
NXOpen.CAM.
InspectionDeltaMoveBuilder
¶ Bases:
NXOpen.CAM.InspectionMoveBuilder
Represents the builder for the CMM Inspection sub-operation Delta Move.
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionDeltaMoveBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the A angle for an indexable head |
AngleB | Returns or sets the B angle for an indexable head |
ApproachDistance | Returns or sets the approach distance |
DeltaX | Returns or sets the delta X coordinate |
DeltaY | Returns or sets the delta Y coordinate |
DeltaZ | Returns or sets the delta Z coordinate |
DepthDistance | Returns or sets the depth distance |
DepthMethod | Returns or sets the depth method |
Intent | Returns or sets the intent |
MotionType | Returns or sets the motion type |
ProbeTipType | Returns or sets the preferred probe tip type |
ProbeTipTypeBuilder | Returns the Probe Tip Type Builder |
RetractDistance | Returns or sets the retract distance |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorStrategy | Returns or sets the sensor selection strategy |
SensorStrategyBuilder | Returns the Sensor Strategy Enum Builder |
Tag | Returns the Tag for this object. |
TipAngleMode | Returns or sets the tip angle selection mode |
TipMode | Returns or sets the probe tip selection mode |
TipNumber | Returns or sets the probe tip number |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetParent | Set parent |
SetProbeAngles | Set default values for probe angles based on feature type. |
SetProbeTip | Set default probe tip based on preferred tip type and probe angles. |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionDeltaMoveBuilderIntentType Enumeration | Move Intent |
Property Detail¶
DeltaX¶
-
InspectionDeltaMoveBuilder.
DeltaX
¶ Returns or sets the delta X coordinate
-------------------------------------
Getter Method
Signature
DeltaX()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaX(deltaX)
Parameters: deltaX (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeltaY¶
-
InspectionDeltaMoveBuilder.
DeltaY
¶ Returns or sets the delta Y coordinate
-------------------------------------
Getter Method
Signature
DeltaY()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaY(deltaY)
Parameters: deltaY (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeltaZ¶
-
InspectionDeltaMoveBuilder.
DeltaZ
¶ Returns or sets the delta Z coordinate
-------------------------------------
Getter Method
Signature
DeltaZ()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeltaZ(deltaZ)
Parameters: deltaZ (float) – New in version NX7.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthDistance¶
-
InspectionDeltaMoveBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance(distance)
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthMethod¶
-
InspectionDeltaMoveBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod()
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod(method)
Parameters: method ( NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Intent¶
-
InspectionDeltaMoveBuilder.
Intent
¶ Returns or sets the intent
-------------------------------------
Getter Method
Signature
Intent()
Returns: Return type: NXOpen.CAM.InspectionDeltaMoveBuilderIntentType
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Intent(intent)
Parameters: intent ( NXOpen.CAM.InspectionDeltaMoveBuilderIntentType
) –New in version NX7.5.2.
License requirements: None.
Method Detail¶
Validate¶
-
InspectionDeltaMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.