InspectionConstructedFeatureBuilderExtractEdgeDistanceType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.ExtractEdgeDistanceType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderExtractEdgeDistanceType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderExtractEdgeDistanceType
¶ Bases:
object
Specifies whether an extract edge distance is absolute part units or a percentage
Enum Members
Enum Member Enum Member Description Absolute Use an absolute distance from edgePercentage Use a percentage distance from edge-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-