InspectionConstructedFeatureBuilderAvailableStateType Enumeration¶
NXOpen.CAM.InspectionConstructedFeatureBuilder.AvailableStateType is an alias for NXOpen.CAM.InspectionConstructedFeatureBuilderAvailableStateType
-
class
NXOpen.CAM.
InspectionConstructedFeatureBuilderAvailableStateType
¶ Bases:
object
State of features in available feature list
Enum Members
Enum Member Enum Member Description Nominal Feature is in its nominal (design) stateActual Feature is an actual measured feature-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-