InspectionCmmCommandBuilderCommandTypes Enumeration¶
NXOpen.CAM.InspectionCmmCommandBuilder.CommandTypes is an alias for NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
-
class
NXOpen.CAM.
InspectionCmmCommandBuilderCommandTypes
¶ Bases:
object
The type of CMM command to be entered
Enum Members
Enum Member Enum Member Description EnterStatement Enter any CMM statementMeasurementMode Enter a statement to set the measurement modeDefineHomePoint Enter a statement defining the home pointMoveMachine Enter a statement to move the machineOutputDecimalPlaces Enter a statement defining the number of decimal places for outputDeclareVariable Enter a statement declaring a variableQISVariable Enter a statement declaring a QIS variablePromptforInput Enter a statement prompting the user for inputProgramLabel Enter a program label statementJumptoLabel Enter a jump to label statementProgramHeader Enter a program header statementSensorSelect Enter a statement defining a sensor selection statementDevice Enter a statement defining a device statementSaveDml Enter a statement defining a Save DML statement-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-