InspectionCircleFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionCircleFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Circle Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCircleFeatureBuilder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
CenterPointX | Returns or sets the circle center point X coordinate |
CenterPointY | Returns or sets the circle center point Y coordinate |
CenterPointZ | Returns or sets the circle center point Z coordinate |
ChannelName | Returns or sets the channel’s name |
CsysRefType | Returns or sets the coordinate system reference type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
CylinderCircleFitModeBuilder | Returns the Cylinder Circle Fitting Mode Builder |
Description | Returns or sets the description |
Diameter | Returns or sets the circle diameter |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InnerOuterType | Returns or sets the inspection feature inner/outer type (hole/pin) |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the circle inspection feature name |
NormalVectorI | Returns or sets the normal vector I component |
NormalVectorJ | Returns or sets the normal vector J component |
NormalVectorK | Returns or sets the normal vector K component |
Notes | Returns the notes builder |
OffsetDistance | Returns the offset distance |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseDirection | Returns or sets the reverse direction button used to flip the normal vector of the circle |
SafeClearance | Returns the safe clearance builder |
SelectProjectionFaces | Returns the button used to select faces to project the circle to |
SelectToolFlag | Returns or sets the user selected tool |
SelectedCircle | Returns the selected circle |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlipNormal | Flips the circle inspection feature normal vector |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
ReverseOffsetDirection | Reverses the offset direction |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateOffset | Updates the circle inspection feature offset distance and associated values |
UpdateParams | Updates circle inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CenterPointX¶
-
InspectionCircleFeatureBuilder.
CenterPointX
¶ Returns or sets the circle center point X coordinate
-------------------------------------
Getter Method
Signature
CenterPointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointX(centerPointX)
Parameters: centerPointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CenterPointY¶
-
InspectionCircleFeatureBuilder.
CenterPointY
¶ Returns or sets the circle center point Y coordinate
-------------------------------------
Getter Method
Signature
CenterPointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointY(centerPointY)
Parameters: centerPointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CenterPointZ¶
-
InspectionCircleFeatureBuilder.
CenterPointZ
¶ Returns or sets the circle center point Z coordinate
-------------------------------------
Getter Method
Signature
CenterPointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointZ(centerPointZ)
Parameters: centerPointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CsysRefType¶
-
InspectionCircleFeatureBuilder.
CsysRefType
¶ Returns or sets the coordinate system reference type
-------------------------------------
Getter Method
Signature
CsysRefType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysRefType(csysRefType)
Parameters: csysRefType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CylinderCircleFitModeBuilder¶
-
InspectionCircleFeatureBuilder.
CylinderCircleFitModeBuilder
¶ Returns the Cylinder Circle Fitting Mode Builder
-------------------------------------
Getter Method
Signature
CylinderCircleFitModeBuilder()
Returns: Return type: NXOpen.CAM.InspectionCylinderCircleFitModeBuilder
New in version NX9.0.0.
License requirements: None.
Diameter¶
-
InspectionCircleFeatureBuilder.
Diameter
¶ Returns or sets the circle diameter
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter(diameter)
Parameters: diameter (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InnerOuterType¶
-
InspectionCircleFeatureBuilder.
InnerOuterType
¶ Returns or sets the inspection feature inner/outer type (hole/pin)
-------------------------------------
Getter Method
Signature
InnerOuterType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationInneroutertypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerOuterType(innerOuterType)
Parameters: innerOuterType ( NXOpen.CAM.CamInspectionOperationInneroutertypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionCircleFeatureBuilder.
Name
¶ Returns or sets the circle inspection feature name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorI¶
-
InspectionCircleFeatureBuilder.
NormalVectorI
¶ Returns or sets the normal vector I component
-------------------------------------
Getter Method
Signature
NormalVectorI()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorI(normalVectorI)
Parameters: normalVectorI (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorJ¶
-
InspectionCircleFeatureBuilder.
NormalVectorJ
¶ Returns or sets the normal vector J component
-------------------------------------
Getter Method
Signature
NormalVectorJ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorJ(normalVectorJ)
Parameters: normalVectorJ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NormalVectorK¶
-
InspectionCircleFeatureBuilder.
NormalVectorK
¶ Returns or sets the normal vector K component
-------------------------------------
Getter Method
Signature
NormalVectorK()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalVectorK(normalVectorK)
Parameters: normalVectorK (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
InspectionCircleFeatureBuilder.
OffsetDistance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
ReverseDirection¶
-
InspectionCircleFeatureBuilder.
ReverseDirection
¶ Returns or sets the reverse direction button used to flip the normal vector of the circle
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectProjectionFaces¶
-
InspectionCircleFeatureBuilder.
SelectProjectionFaces
¶ Returns the button used to select faces to project the circle to
-------------------------------------
Getter Method
Signature
SelectProjectionFaces()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
SelectedCircle¶
-
InspectionCircleFeatureBuilder.
SelectedCircle
¶ Returns the selected circle
-------------------------------------
Getter Method
Signature
SelectedCircle()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Method Detail¶
FlipNormal¶
-
InspectionCircleFeatureBuilder.
FlipNormal
¶ Flips the circle inspection feature normal vector
Signature
FlipNormal()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseOffsetDirection¶
-
InspectionCircleFeatureBuilder.
ReverseOffsetDirection
¶ Reverses the offset direction
Signature
ReverseOffsetDirection()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateOffset¶
-
InspectionCircleFeatureBuilder.
UpdateOffset
¶ Updates the circle inspection feature offset distance and associated values
Signature
UpdateOffset()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionCircleFeatureBuilder.
UpdateParams
¶ Updates circle inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCircleFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.