HoleDrillingBuilder Class¶
-
class
NXOpen.CAM.
HoleDrillingBuilder
¶ Bases:
NXOpen.CAM.HoleMachiningBuilder
Represents a HoleDrillingBuilder Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateHoleDrillingBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CollisionCheck | Returns or sets the collision check for cutting |
CutParameters | Returns the Hole Drilling Cut Parameters |
CuttingParameters | Returns the Cut Parameters |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IgnoreToolTip | Returns or sets the ignore tool tip flag |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting moves builder |
Notes | Returns the notes builder |
OppositeDirection | Returns the opposite direction |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeatureGeometry | Returns the feature geometry @return |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CutParameters¶
-
HoleDrillingBuilder.
CutParameters
¶ Returns the Hole Drilling Cut Parameters
-------------------------------------
Getter Method
Signature
CutParameters()
Returns: the Cut Parameters Return type: NXOpen.CAM.HoleDrillingCutParameters
New in version NX9.0.0.
Deprecated since version NX9.0.3: Use
CAM.HoleMachiningBuilder.CuttingParameters
instead.License requirements: None.
IgnoreToolTip¶
-
HoleDrillingBuilder.
IgnoreToolTip
¶ Returns or sets the ignore tool tip flag
-------------------------------------
Getter Method
Signature
IgnoreToolTip()
Returns: the ignore tool tip flag Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
IgnoreToolTip(flag)
Parameters: flag (bool) – the ignore tool tip flag New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
OppositeDirection¶
-
HoleDrillingBuilder.
OppositeDirection
¶ Returns the opposite direction
-------------------------------------
Getter Method
Signature
OppositeDirection()
Returns: the opposite direction Return type: NXOpen.CAM.OppositeDirection
New in version NX9.0.0.
Deprecated since version NX9.0.2: Change the Z-axis of the in-process feature instead.
License requirements: None.
Method Detail¶
Validate¶
-
HoleDrillingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.