GrooveMillingBuilderLevelSequencingType Enumeration¶
NXOpen.CAM.GrooveMillingBuilder.LevelSequencingType is an alias for NXOpen.CAM.GrooveMillingBuilderLevelSequencingType
-
class
NXOpen.CAM.
GrooveMillingBuilderLevelSequencingType
¶ Bases:
object
Available types for level sequencing
Enum Members
Enum Member Enum Member Description CeilingToFloor Ceiling to FloorFloorToCeiling Floor to CeilingCenterCeilingFloor Start in Center then Ceiling then FloorCenterFloorCeiling Start in Center then Floor then CeilingCenterAlternateCeilingFirst Center Alternate, Ceiling FirstCenterAlternateFloorFirst Center Alternate, Floor First-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-