FeedsBuilderRecalcuateBasedOn Enumeration¶
NXOpen.CAM.FeedsBuilder.RecalcuateBasedOn is an alias for NXOpen.CAM.FeedsBuilderRecalcuateBasedOn
-
class
NXOpen.CAM.
FeedsBuilderRecalcuateBasedOn
¶ Bases:
object
The recalculation based on attribute
New in version NX8.0.0.
Enum Members
Enum Member Enum Member Description SurfaceSpeed surface speedSpindleSpeed spindle speedFeedPerTooth feed per toothCutFeedRate cut feed rate-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-