FeedStatusData Struct¶
-
class
NXOpen.CAM.
FeedStatusData
¶ Bases:
object
The data for CamUI_FeedStatusComp
New in version NX5.0.0.
Fields¶
Field | Description |
---|---|
Value | double value |
Unit | feed rate unit |
Inheritance | inheritance status |
Value¶
-
FeedStatusData.
Value
¶ double value
-------------------------------------
Getter Method Signature
Value()
Returns: Return type: float -------------------------------------
Setter Method
Signature
Value(value)
Parameters: value (float) –
Unit¶
-
FeedStatusData.
Unit
¶ feed rate unit
-------------------------------------
Getter Method Signature
Unit()
Returns: Return type: NXOpen.CAM.FeedRateUnit
-------------------------------------
Setter Method
Signature
Unit(value)
Parameters: value ( NXOpen.CAM.FeedRateUnit
) –
Inheritance¶
-
FeedStatusData.
Inheritance
¶ inheritance status
-------------------------------------
Getter Method Signature
Inheritance()
Returns: Return type: NXOpen.CAM.Inheritance
-------------------------------------
Setter Method
Signature
Inheritance(value)
Parameters: value ( NXOpen.CAM.Inheritance
) –