ThreadFeatureGeometry Class¶
-
class
NXOpen.CAM.FBM.
ThreadFeatureGeometry
¶ Bases:
NXOpen.CAM.FBM.FeatureGeometry
Represents a feature geometry builder
This is an abstract class and cannot be instantiated.
New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
FormStandard | Returns or sets the form standard |
GeometryList | Returns the geometry list |
Tag | Returns the Tag for this object. |
ThreadRotation | Returns or sets the thread rotation |
Topology | Returns the topology builder |
Methods¶
Method | Description |
---|---|
AddFeatureSet | Creates a feature geometry set @return the new in process feature set |
AppendGeometrySet | Append an geometry set with dumb rules @return the appended geometry set object |
CreateFeatureSet | Create a new empty feature editor @return the new in process feature set |
CreateGeometrySet | Create an empty geometry set @return the geometry set object |
ExpandSets | Expanding the geometry sets |
GetFeatureSet | Get the in process feature editor at the specified index @return the in process feature set |
GetFormUserDefined | Get the user defined form standard @return |
GetMachiningArea | Returns the machining area @return the machining area |
GetThreadDataSource | Gets the source type for retrieving thread data @return thread data source type |
InitializeData | Prepare and update geometry data |
PreselectGeometry | Pre-select the wall geometry |
ReloadList | Reload list from parent |
ReorderFeatures | Reorders the features according to a predefined algorithm |
ReorderFeaturesByDirection | Reorders the features according to primary direction |
ReverseFeatures | Reverse the features |
SetDefaultAttribute | Sets a default attribute value |
SetFormUserDefined | Set the user defined form standard |
SetMachiningArea | Change machining area |
SetThreadDataSource | Sets the source type for retrieving thread data |
UpdateThreadParameters | Update the feature thread parameters |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ThreadFeatureGeometryForm Enumeration | Thread form standards |
ThreadFeatureGeometryRotation Enumeration | the rotation types |
ThreadFeatureGeometryThreadDataSource Enumeration | thread data source types |
Property Detail¶
FormStandard¶
-
ThreadFeatureGeometry.
FormStandard
¶ Returns or sets the form standard
-------------------------------------
Getter Method
Signature
FormStandard()
Returns: form standard Return type: NXOpen.CAM.FBM.ThreadFeatureGeometryForm
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FormStandard(standard)
Parameters: standard ( NXOpen.CAM.FBM.ThreadFeatureGeometryForm
) – form standardNew in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
ThreadRotation¶
-
ThreadFeatureGeometry.
ThreadRotation
¶ Returns or sets the thread rotation
-------------------------------------
Getter Method
Signature
ThreadRotation()
Returns: thread rotation Return type: NXOpen.CAM.FBM.ThreadFeatureGeometryRotation
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThreadRotation(rotation)
Parameters: rotation ( NXOpen.CAM.FBM.ThreadFeatureGeometryRotation
) – thread rotationNew in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetFormUserDefined¶
-
ThreadFeatureGeometry.
GetFormUserDefined
¶ Get the user defined form standard
Signature
GetFormUserDefined()
Returns: Return type: str New in version NX9.0.2.
License requirements: None.
GetThreadDataSource¶
-
ThreadFeatureGeometry.
GetThreadDataSource
¶ Gets the source type for retrieving thread data
Signature
GetThreadDataSource()
Returns: thread data source type Return type: NXOpen.CAM.FBM.ThreadFeatureGeometryThreadDataSource
New in version NX9.0.1.
License requirements: None.
SetFormUserDefined¶
-
ThreadFeatureGeometry.
SetFormUserDefined
¶ Set the user defined form standard
Signature
SetFormUserDefined(userDefinedForm)
Parameters: userDefinedForm (str) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
SetThreadDataSource¶
-
ThreadFeatureGeometry.
SetThreadDataSource
¶ Sets the source type for retrieving thread data
Signature
SetThreadDataSource(source)
Parameters: source ( NXOpen.CAM.FBM.ThreadFeatureGeometryThreadDataSource
) – thread data source typeNew in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
UpdateThreadParameters¶
-
ThreadFeatureGeometry.
UpdateThreadParameters
¶ Update the feature thread parameters
Signature
UpdateThreadParameters(tagFeature)
Parameters: tagFeature ( NXOpen.CAM.FBM.Feature
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
ThreadFeatureGeometry.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.