MachiningFeatureGeometry Class¶
-
class
NXOpen.CAM.FBM.
MachiningFeatureGeometry
¶ Bases:
NXOpen.CAM.FBM.FeatureGeometry
Represents a feature geometry builder
An instance of this class can be obtained from
CAM.HoleBossGeom.GetCenterHoleGeometry
orCAM.HoleBossGeom.GetChamferHoleGeometry
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
GeometryList | Returns the geometry list |
Tag | Returns the Tag for this object. |
Topology | Returns the topology builder |
Methods¶
Method | Description |
---|---|
AddFeatureSet | Creates a feature geometry set @return the new in process feature set |
AppendGeometrySet | Append an geometry set with dumb rules @return the appended geometry set object |
CreateFeatureSet | Create a new empty feature editor @return the new in process feature set |
CreateGeometrySet | Create an empty geometry set @return the geometry set object |
ExpandSets | Expanding the geometry sets |
GetFeatureSet | Get the in process feature editor at the specified index @return the in process feature set |
GetMachiningArea | Returns the machining area @return the machining area |
InitializeData | Prepare and update geometry data |
PreselectGeometry | Pre-select the wall geometry |
ReloadList | Reload list from parent |
ReorderFeatures | Reorders the features according to a predefined algorithm |
ReorderFeaturesByDirection | Reorders the features according to primary direction |
ReverseFeatures | Reverse the features |
SetDefaultAttribute | Sets a default attribute value |
SetMachiningArea | Change machining area |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
MachiningFeatureGeometry.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.