EditSubopCommand Class¶
-
class
NXOpen.CAM.
EditSubopCommand
¶ Bases:
NXOpen.TaggedObject
Represents an Edit Subop Command Builder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ContainmentType | Returns or sets the containment type |
PointType | Returns or sets the point type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetStartPoints | Get the start point value |
SetStartPoints | Set the start point value |
Enumerations¶
EditSubopCommandContainmentTypes Enumeration | Available types for containment |
EditSubopCommandPointTypes Enumeration | Available types for point |
Property Detail¶
ContainmentType¶
-
EditSubopCommand.
ContainmentType
¶ Returns or sets the containment type
-------------------------------------
Getter Method
Signature
ContainmentType()
Returns: the containment type value Return type: NXOpen.CAM.EditSubopCommandContainmentTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContainmentType(containmentType)
Parameters: containmentType ( NXOpen.CAM.EditSubopCommandContainmentTypes
) – the containment type valueNew in version NX9.0.0.
License requirements: None.
PointType¶
-
EditSubopCommand.
PointType
¶ Returns or sets the point type
-------------------------------------
Getter Method
Signature
PointType()
Returns: the point type value Return type: NXOpen.CAM.EditSubopCommandPointTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointType(pointType)
Parameters: pointType ( NXOpen.CAM.EditSubopCommandPointTypes
) – the point type valueNew in version NX9.0.0.
License requirements: None.
Method Detail¶
GetStartPoints¶
-
EditSubopCommand.
GetStartPoints
¶ Get the start point value
Signature
GetStartPoints()
Returns: the start point value Return type: list of NXOpen.Point
New in version NX9.0.0.
License requirements: None.
SetStartPoints¶
-
EditSubopCommand.
SetStartPoints
¶ Set the start point value
Signature
SetStartPoints(startPoint)
Parameters: startPoint (list of NXOpen.Point
) – the start point valueNew in version NX9.0.0.
License requirements: None.