DmTpBuilder Class¶
-
class
NXOpen.CAM.
DmTpBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a tool path Drive Method Builder
This is an abstract class and cannot be instantiated.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
SpecifyClsf | Specifies the clsf file, including both the directory path and file name. |
SpecifyToolPath | Specifies the tool path name. |
Method Detail¶
SpecifyClsf¶
-
DmTpBuilder.
SpecifyClsf
¶ Specifies the clsf file, including both the directory path and file name.
Signature
SpecifyClsf(clsfFileName)
Parameters: clsfFileName (str) – the clsf file name NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SpecifyToolPath¶
-
DmTpBuilder.
SpecifyToolPath
¶ Specifies the tool path name.
Signature
SpecifyToolPath(toolPathName)
Parameters: toolPathName (str) – the tool path name NOTE: The full Unicode character set is not supported for this parameter. New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)