DmSurfBuilderGougeActionType Enumeration¶
NXOpen.CAM.DmSurfBuilder.GougeActionType is an alias for NXOpen.CAM.DmSurfBuilderGougeActionType
-
class
NXOpen.CAM.
DmSurfBuilderGougeActionType
¶ Bases:
object
Surface Drive method/Gouge Check in scop
Enum Members
Enum Member Enum Member Description None None Warning Warning Skip Skip Retract Retract -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-