DmSurfBuilderCutDirection Enumeration¶
NXOpen.CAM.DmSurfBuilder.CutDirection is an alias for NXOpen.CAM.DmSurfBuilderCutDirection
-
class
NXOpen.CAM.
DmSurfBuilderCutDirection
¶ Bases:
object
Available types for Cut Direction
Enum Members
Enum Member Enum Member Description Corner1U Corner 1 U direction Corner1V Corner 1 V direction Corner2U Corner 2 U direction Corner2V Corner 2 V direction Corner3U Corner 3 U direction Corner3V Corner 3 V direction Corner4U Corner 4 U direction Corner4V Corner 4 V direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-