DmSpiralBuilder Class¶
-
class
NXOpen.CAM.
DmSpiralBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a Spiral Drive Method Builder
This is an abstract class and cannot be instantiated.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DmSpiralStepoverMenu | Returns or sets the Spiral Drive Method Stepover type. |
PatternCenterPoint | Returns or sets the Pattern Center Point |
SpiralRadiusBuilder | Returns the Spiral Radius |
SpiralStepoverBuilder | Returns the Spiral Stepover builder |
SpiralStepoverDistance | Returns or sets the Stepover Distance. |
SpiralStepoverPercent | Returns or sets the Stepover Percent. |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
DmSpiralBuilderDmSpiralStepoverTypes Enumeration | Available types for Spiral drive method stepover in SurfaceContour. |
Property Detail¶
PatternCenterPoint¶
-
DmSpiralBuilder.
PatternCenterPoint
¶ Returns or sets the Pattern Center Point
-------------------------------------
Getter Method
Signature
PatternCenterPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PatternCenterPoint(centerPoint)
Parameters: centerPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SpiralRadiusBuilder¶
-
DmSpiralBuilder.
SpiralRadiusBuilder
¶ Returns the Spiral Radius
-------------------------------------
Getter Method
Signature
SpiralRadiusBuilder()
Returns: the spiral radius value Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX5.0.0.
License requirements: None.
SpiralStepoverBuilder¶
-
DmSpiralBuilder.
SpiralStepoverBuilder
¶ Returns the Spiral Stepover builder
-------------------------------------
Getter Method
Signature
SpiralStepoverBuilder()
Returns: the spiral stepover builder Return type: NXOpen.CAM.StepoverBuilder
New in version NX6.0.0.
License requirements: None.
SpiralStepoverDistance¶
-
DmSpiralBuilder.
SpiralStepoverDistance
¶ Returns or sets the Stepover Distance.
This property is obsolete.
-------------------------------------
Getter Method
Signature
SpiralStepoverDistance()
Returns: the Stepover Distance Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpiralStepoverDistance(stepoverDist)
Parameters: stepoverDist (float) – the Stepover Distance New in version NX5.0.0.
License requirements: None.
SpiralStepoverPercent¶
-
DmSpiralBuilder.
SpiralStepoverPercent
¶ Returns or sets the Stepover Percent.
This property is obsolete.
-------------------------------------
Getter Method
Signature
SpiralStepoverPercent()
Returns: the Stepover Percent Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpiralStepoverPercent(stepoverPercent)
Parameters: stepoverPercent (float) – the Stepover Percent New in version NX5.0.0.
License requirements: None.