CylinderMillingBuilderDiameterForHelixTypes Enumeration¶
NXOpen.CAM.CylinderMillingBuilder.DiameterForHelixTypes is an alias for NXOpen.CAM.CylinderMillingBuilderDiameterForHelixTypes
-
class
NXOpen.CAM.
CylinderMillingBuilderDiameterForHelixTypes
¶ Bases:
object
Diameter for Helix
New in version NX8.0.0.
Enum Members
Enum Member Enum Member Description Diameter Helix DiameterSpiralThickness Spiral ThicknessOffsetFromStartDiameter Offset from Start Diameter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-