CutPatternBuilderTypes Enumeration¶
NXOpen.CAM.CutPatternBuilder.Types is an alias for NXOpen.CAM.CutPatternBuilderTypes
-
class
NXOpen.CAM.
CutPatternBuilderTypes
¶ Bases:
object
cut pattern options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description None NoneFollowPart Follow PartFollowPeriphery Follow PeripheryHelical HelicalSpiral SpiralHelicalSpiral Helical or SpiralMixed MixedProfile ProfileStandardDrive Standard DriveTrochoidal TrochoidalZig ZigZigZag Zig ZagZigZagWithLifts Zig Zag with LiftsZigWithContour Zig with ContourZigWithStepover Zig with StepoverConcentricZig Concentric ZigConcentricZigZag Concentric Zig ZagConcentricZigWithContour Concentric Zig with ContourConcentricZigWithStepover Concentric Zig with StepoverRadialZig Radial ZigRadialZigZag Radial Zig ZagRadialZigZagWithLifts Radial Zig Zag with LiftsRadialZigWithContour Radial Zig with ContourRadialZigWithStepover Radial Zig with StepoverCrosscutZig Crosscut ZigCrosscutZigZag Crosscut Zig ZagCrosscutZigZagWithLifts Crosscut Zig Zag with LiftsZlevelZig Zlevel ZigZlevelZigZag Zlevel Zig ZagZlevelZigZagWithLifts Zlevel Zig Zag with LiftsSameAsNonSteep Same as Non-steep-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-