CutParametersExtendAtStartMode Enumeration¶
-
class
NXOpen.CAM.
CutParametersExtendAtStartMode
¶ Bases:
object
Available modes for Turning Cutting Corners Extend At Start
New in version NX8.5.0.
Enum Members
Enum Member Enum Member Description None NoneToContainmentGeometry To Containment GeometryIncludeAdjacentChamfersOrRounds Include Adjacent Chamfers or Rounds-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-