CutDepthChecker Class

class NXOpen.CAM.CutDepthChecker

Bases: NXOpen.Builder

Represents a cut depth checker object

This has not creator

New in version NX8.5.0.

Properties

Property Description
CheckNeck Returns or sets the indicator to include tool neck in the collision check process
CreateCurvesForGouges Returns or sets the indicator to create curves for the gouged motions
CutVolume Returns the calculated cut volume
DisplayGouges Returns or sets the indicator to display gouges
MaxCutDepthViolation Returns the maximum cut depth violation
NumCutDepthViolations Returns the number of cut depth violations
OperationToCheck Returns or sets the operation that is being checked
PauseOnGouge Returns or sets the indicator for pausing on gouge
StopLimit Returns or sets the number of gouges to be used as a limit to stop
StopOnLimit Returns or sets the indicator to stop when the number of gouges has equalled the stop limit
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
PerformCheck The action to perform the check
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CheckNeck

CutDepthChecker.CheckNeck

Returns or sets the indicator to include tool neck in the collision check process

-------------------------------------

Getter Method

Signature CheckNeck()

Returns:indicator to include tool neck in the collision check process
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CheckNeck(newValue)

Parameters:newValue (bool) – indicator to include tool neck in the collision check process

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

CreateCurvesForGouges

CutDepthChecker.CreateCurvesForGouges

Returns or sets the indicator to create curves for the gouged motions

-------------------------------------

Getter Method

Signature CreateCurvesForGouges()

Returns:indicator to create curves for the gouged motions
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CreateCurvesForGouges(newValue)

Parameters:newValue (bool) – indicator to create curves for the gouged motions

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

CutVolume

CutDepthChecker.CutVolume

Returns the calculated cut volume

-------------------------------------

Getter Method

Signature CutVolume()

Returns:calculated cut volume
Return type:float

New in version NX8.5.0.

License requirements: None.

DisplayGouges

CutDepthChecker.DisplayGouges

Returns or sets the indicator to display gouges

-------------------------------------

Getter Method

Signature DisplayGouges()

Returns:indicator to display gouges
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DisplayGouges(newValue)

Parameters:newValue (bool) – indicator to display gouges

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

MaxCutDepthViolation

CutDepthChecker.MaxCutDepthViolation

Returns the maximum cut depth violation

-------------------------------------

Getter Method

Signature MaxCutDepthViolation()

Returns:the maximum cut depth violation
Return type:float

New in version NX8.5.0.

License requirements: None.

NumCutDepthViolations

CutDepthChecker.NumCutDepthViolations

Returns the number of cut depth violations

-------------------------------------

Getter Method

Signature NumCutDepthViolations()

Returns:the number of cut depth violations
Return type:int

New in version NX8.5.0.

License requirements: None.

OperationToCheck

CutDepthChecker.OperationToCheck

Returns or sets the operation that is being checked

-------------------------------------

Getter Method

Signature OperationToCheck()

Returns:the operation which has to be checked
Return type:NXOpen.CAM.Operation

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OperationToCheck(operation)

Parameters:operation (NXOpen.CAM.Operation) – the operation which has to be checked

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

PauseOnGouge

CutDepthChecker.PauseOnGouge

Returns or sets the indicator for pausing on gouge

-------------------------------------

Getter Method

Signature PauseOnGouge()

Returns:indicator for pausing on gouge
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PauseOnGouge(newValue)

Parameters:newValue (bool) – indicator for pausing on gouge

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

StopLimit

CutDepthChecker.StopLimit

Returns or sets the number of gouges to be used as a limit to stop

-------------------------------------

Getter Method

Signature StopLimit()

Returns:the number of gouges to be used as a limit to stop
Return type:int

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StopLimit(newValue)

Parameters:newValue (int) – the number of gouges to be used as a limit to stop

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

StopOnLimit

CutDepthChecker.StopOnLimit

Returns or sets the indicator to stop when the number of gouges has equalled the stop limit

-------------------------------------

Getter Method

Signature StopOnLimit()

Returns:the number of gouges to be used as a limit to stop
Return type:bool

New in version NX8.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature StopOnLimit(newValue)

Parameters:newValue (bool) – the number of gouges to be used as a limit to stop

New in version NX8.5.0.

License requirements: cam_base (“CAM BASE”)

Method Detail

PerformCheck

CutDepthChecker.PerformCheck

The action to perform the check

Signature PerformCheck()

New in version NX8.5.0.

License requirements: None.

Validate

CutDepthChecker.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.