BoundaryTurnMemberOffset Class¶
-
class
NXOpen.CAM.
BoundaryTurnMemberOffset
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.BoundaryTurnMemberOffset
This builder cannot be instantiated separately.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
AxialDistance | Returns or sets the offset axial distance |
Distance | Returns or sets the offset distance (general and legacy) |
DistanceType | Returns or sets the offset distance type (general and legacy) |
EndDistance | Returns or sets the offset end distance (conical) |
Method | Returns or sets the offset method |
Mode | Returns or sets the offset mode |
RadialDistance | Returns or sets the offset radial distance |
StartDistance | Returns or sets the offset start distance (conical) |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the offset vector |
VectorDistance | Returns or sets the offset vecot distance |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundaryTurnMemberOffsetDistanceTypeMode Enumeration | the types available for member distance |
BoundaryTurnMemberOffsetMethodType Enumeration | the types available for member offset method |
BoundaryTurnMemberOffsetModeType Enumeration | the types available for member offset mode |
Property Detail¶
AxialDistance¶
-
BoundaryTurnMemberOffset.
AxialDistance
¶ Returns or sets the offset axial distance
-------------------------------------
Getter Method
Signature
AxialDistance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxialDistance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Distance¶
-
BoundaryTurnMemberOffset.
Distance
¶ Returns or sets the offset distance (general and legacy)
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
DistanceType¶
-
BoundaryTurnMemberOffset.
DistanceType
¶ Returns or sets the offset distance type (general and legacy)
-------------------------------------
Getter Method
Signature
DistanceType()
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberOffsetDistanceTypeMode
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceType(newValue)
Parameters: newValue ( NXOpen.CAM.BoundaryTurnMemberOffsetDistanceTypeMode
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
EndDistance¶
-
BoundaryTurnMemberOffset.
EndDistance
¶ Returns or sets the offset end distance (conical)
-------------------------------------
Getter Method
Signature
EndDistance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDistance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method¶
-
BoundaryTurnMemberOffset.
Method
¶ Returns or sets the offset method
-------------------------------------
Getter Method
Signature
Method()
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberOffsetMethodType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Method(newValue)
Parameters: newValue ( NXOpen.CAM.BoundaryTurnMemberOffsetMethodType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Mode¶
-
BoundaryTurnMemberOffset.
Mode
¶ Returns or sets the offset mode
-------------------------------------
Getter Method
Signature
Mode()
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberOffsetModeType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Mode(newValue)
Parameters: newValue ( NXOpen.CAM.BoundaryTurnMemberOffsetModeType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
RadialDistance¶
-
BoundaryTurnMemberOffset.
RadialDistance
¶ Returns or sets the offset radial distance
-------------------------------------
Getter Method
Signature
RadialDistance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialDistance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
StartDistance¶
-
BoundaryTurnMemberOffset.
StartDistance
¶ Returns or sets the offset start distance (conical)
-------------------------------------
Getter Method
Signature
StartDistance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDistance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Vector¶
-
BoundaryTurnMemberOffset.
Vector
¶ Returns or sets the offset vector
-------------------------------------
Getter Method
Signature
Vector()
Returns: vector Return type: NXOpen.NXObject
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(newValue)
Parameters: newValue ( NXOpen.NXObject
) – vectorNew in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
VectorDistance¶
-
BoundaryTurnMemberOffset.
VectorDistance
¶ Returns or sets the offset vecot distance
-------------------------------------
Getter Method
Signature
VectorDistance()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorDistance(newValue)
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
BoundaryTurnMemberOffset.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.