BoundaryTurnBlank Class¶
-
class
NXOpen.CAM.
BoundaryTurnBlank
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.BoundaryTurnBlank
This builder cannot be instantiated separately.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
AutoPosition | Returns or sets the automatic position flag |
BlankType | Returns or sets the workpiece type |
Boundary | Returns the boundary |
Diameter | Returns or sets the diameter of the bar |
EquidistantStock | Returns or sets the equidistant stock |
FaceStock | Returns or sets the face stock |
FlipDirection | Returns or sets the flip direction flag |
InnerDiameter | Returns or sets the inner diameter of the tube |
Length | Returns or sets the length of the bar or tube |
MountingPosition | Returns or sets the mounting position |
OuterDiameter | Returns or sets the outer diameter of the tube |
Point | Returns or sets the head stock position |
RadialStock | Returns or sets the radial stock |
ReferencePoint | Returns or sets the reference point |
Tag | Returns the Tag for this object. |
TargetPoint | Returns or sets the target point |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundaryTurnBlankPosition Enumeration | the mounting direction types available |
BoundaryTurnBlankType Enumeration | the blank types available |
Property Detail¶
AutoPosition¶
-
BoundaryTurnBlank.
AutoPosition
¶ Returns or sets the automatic position flag
-------------------------------------
Getter Method
Signature
AutoPosition()
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoPosition(autoPosition)
Parameters: autoPosition (bool) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
BlankType¶
-
BoundaryTurnBlank.
BlankType
¶ Returns or sets the workpiece type
-------------------------------------
Getter Method
Signature
BlankType()
Returns: Return type: NXOpen.CAM.BoundaryTurnBlankType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankType(stockType)
Parameters: stockType ( NXOpen.CAM.BoundaryTurnBlankType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Boundary¶
-
BoundaryTurnBlank.
Boundary
¶ Returns the boundary
-------------------------------------
Getter Method
Signature
Boundary()
Returns: Return type: NXOpen.CAM.Boundary
New in version NX9.0.2.
License requirements: None.
Diameter¶
-
BoundaryTurnBlank.
Diameter
¶ Returns or sets the diameter of the bar
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter(diameter)
Parameters: diameter (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
EquidistantStock¶
-
BoundaryTurnBlank.
EquidistantStock
¶ Returns or sets the equidistant stock
-------------------------------------
Getter Method
Signature
EquidistantStock()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
EquidistantStock(equidistantStock)
Parameters: equidistantStock (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FaceStock¶
-
BoundaryTurnBlank.
FaceStock
¶ Returns or sets the face stock
-------------------------------------
Getter Method
Signature
FaceStock()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceStock(faceStock)
Parameters: faceStock (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FlipDirection¶
-
BoundaryTurnBlank.
FlipDirection
¶ Returns or sets the flip direction flag
-------------------------------------
Getter Method
Signature
FlipDirection()
Returns: Return type: bool New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipDirection(flipDirection)
Parameters: flipDirection (bool) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
InnerDiameter¶
-
BoundaryTurnBlank.
InnerDiameter
¶ Returns or sets the inner diameter of the tube
-------------------------------------
Getter Method
Signature
InnerDiameter()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerDiameter(innerDiameter)
Parameters: innerDiameter (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Length¶
-
BoundaryTurnBlank.
Length
¶ Returns or sets the length of the bar or tube
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length(length)
Parameters: length (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
MountingPosition¶
-
BoundaryTurnBlank.
MountingPosition
¶ Returns or sets the mounting position
-------------------------------------
Getter Method
Signature
MountingPosition()
Returns: Return type: NXOpen.CAM.BoundaryTurnBlankPosition
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
MountingPosition(mountPos)
Parameters: mountPos ( NXOpen.CAM.BoundaryTurnBlankPosition
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
OuterDiameter¶
-
BoundaryTurnBlank.
OuterDiameter
¶ Returns or sets the outer diameter of the tube
-------------------------------------
Getter Method
Signature
OuterDiameter()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
OuterDiameter(outerDiameter)
Parameters: outerDiameter (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Point¶
-
BoundaryTurnBlank.
Point
¶ Returns or sets the head stock position
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(headStockPosition)
Parameters: headStockPosition ( NXOpen.Point
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
RadialStock¶
-
BoundaryTurnBlank.
RadialStock
¶ Returns or sets the radial stock
-------------------------------------
Getter Method
Signature
RadialStock()
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialStock(radialStock)
Parameters: radialStock (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
ReferencePoint¶
-
BoundaryTurnBlank.
ReferencePoint
¶ Returns or sets the reference point
-------------------------------------
Getter Method
Signature
ReferencePoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePoint(referencePoint)
Parameters: referencePoint ( NXOpen.Point
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
TargetPoint¶
-
BoundaryTurnBlank.
TargetPoint
¶ Returns or sets the target point
-------------------------------------
Getter Method
Signature
TargetPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetPoint(targetPoint)
Parameters: targetPoint ( NXOpen.Point
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
BoundaryTurnBlank.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.