BoundarySetToolSideTypes Enumeration¶
NXOpen.CAM.BoundarySet.ToolSideTypes is an alias for NXOpen.CAM.BoundarySetToolSideTypes
-
class
NXOpen.CAM.
BoundarySetToolSideTypes
¶ Bases:
object
the tool side types
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description InsideOrLeft inside for closed boundary, or left side for open boundaryOutsideOrRight outside for closed boundary, or right side for open boundary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-