BoundaryMillingMemberSetFeedUnitTypes Enumeration¶
NXOpen.CAM.BoundaryMillingMemberSet.FeedUnitTypes is an alias for NXOpen.CAM.BoundaryMillingMemberSetFeedUnitTypes
-
class
NXOpen.CAM.
BoundaryMillingMemberSetFeedUnitTypes
¶ Bases:
object
the types available for the feed rate unit
Enum Members
Enum Member Enum Member Description None no feed rate unitPerMinute use per minute as the feed rate unitPerRevolution use per revolution as the feed rate unit-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-