BoundaryMemberSet Class¶
-
class
NXOpen.CAM.
BoundaryMemberSet
¶ Bases:
NXOpen.TaggedObject
Represents a boundary member set .
To create a new instance of this class, use
NXOpen.CAM.BoundarySet.CreateBoundaryMemberSet
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConnectMember | Returns or sets the connect member |
CustomOffset | Returns or sets the flag whether this boundary has custom offset activated |
Offset | Returns or sets the offset value |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
BoundaryMemberSetConnectMemberType Enumeration | the types available for connect member |
Property Detail¶
ConnectMember¶
-
BoundaryMemberSet.
ConnectMember
¶ Returns or sets the connect member
-------------------------------------
Getter Method
Signature
ConnectMember()
Returns: Return type: NXOpen.CAM.BoundaryMemberSetConnectMemberType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConnectMember(newValue)
Parameters: newValue ( NXOpen.CAM.BoundaryMemberSetConnectMemberType
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CustomOffset¶
-
BoundaryMemberSet.
CustomOffset
¶ Returns or sets the flag whether this boundary has custom offset activated
-------------------------------------
Getter Method
Signature
CustomOffset()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomOffset(newValue)
Parameters: newValue (bool) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Offset¶
-
BoundaryMemberSet.
Offset
¶ Returns or sets the offset value
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Offset(newValue)
Parameters: newValue (float) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)