PlotParameters Class¶
-
class
NXOpen.CAE.Xyplot.
PlotParameters
¶ Bases:
NXOpen.CAE.Xyplot.BasePlotParameters
Represents the parameters passed to create a plot.
To create a new instance of this class, use
NXOpen.CAE.Xyplot.XYPlotManager.NewPlotParameters
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
DeviceIndex | Returns or sets the index of device on which plot graph will be shown. |
GraphTemplate | Returns the graph template to be used by the plot |
Is2DPlot | Returns or sets the value indicates whether to create a 2D plot |
PlotTemplate | Returns the plot template to be used by the plot |
PlotType | Returns or sets the plot type |
ViewPortIndex | Returns or sets the index of a view port on main graphic window, on which plot graph will be shown. |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
GetRecords | Gets the records to be plotted @return Records |
SetRecords | Sets the records to be plotted |
Property Detail¶
GraphTemplate¶
-
PlotParameters.
GraphTemplate
¶ Returns the graph template to be used by the plot
-------------------------------------
Getter Method
Signature
GraphTemplate()
Returns: Return type: NXOpen.CAE.Xyplot.BaseTemplate
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
CAE.Xyplot.PlotParameters.PlotTemplate
instead.License requirements: None.
Is2DPlot¶
-
PlotParameters.
Is2DPlot
¶ Returns or sets the value indicates whether to create a 2D plot
-------------------------------------
Getter Method
Signature
Is2DPlot()
Returns: Return type: bool New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
CAE.Xyplot.PlotParameters.PlotType
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Is2DPlot(is2DPlot)
Parameters: is2DPlot (bool) – New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
CAE.Xyplot.PlotParameters.PlotType
instead.License requirements: None.
PlotTemplate¶
-
PlotParameters.
PlotTemplate
¶ Returns the plot template to be used by the plot
-------------------------------------
Getter Method
Signature
PlotTemplate()
Returns: Return type: NXOpen.CAE.Xyplot.PlotGraphTemplate
New in version NX10.0.0.
License requirements: None.
PlotType¶
-
PlotParameters.
PlotType
¶ Returns or sets the plot type
-------------------------------------
Getter Method
Signature
PlotType()
Returns: Return type: NXOpen.CAE.Xyplot.PlotType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlotType(plotType)
Parameters: plotType ( NXOpen.CAE.Xyplot.PlotType
) –New in version NX10.0.0.
License requirements: None.