GeneralDisplayStyles Class¶
-
class
NXOpen.CAE.Xyplot.
GeneralDisplayStyles
¶ Bases:
NXOpen.TaggedObject
,NXOpen.CAE.Xyplot.IDisplayStyle
Manages the general display styles.
Not support KF.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Owner | Returns the owner style |
PhaseAngle | Returns or sets the phase angle in degree |
PhaseRangeOption | Returns or sets the phase range option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CommitChange | Commits any edits that have been applied to the display style. |
Property Detail¶
Owner¶
-
GeneralDisplayStyles.
Owner
¶ Returns the owner style
-------------------------------------
Getter Method
Signature
Owner()
Returns: Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: None.
PhaseAngle¶
-
GeneralDisplayStyles.
PhaseAngle
¶ Returns or sets the phase angle in degree
-------------------------------------
Getter Method
Signature
PhaseAngle()
Returns: Phase angle Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PhaseAngle(phaseAngle)
Parameters: phaseAngle (float) – Phase angle New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
PhaseRangeOption¶
-
GeneralDisplayStyles.
PhaseRangeOption
¶ Returns or sets the phase range option
-------------------------------------
Getter Method
Signature
PhaseRangeOption()
Returns: Phase range option Return type: NXOpen.CAE.Xyplot.PhaseRangeOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PhaseRangeOption(phaseRangeOption)
Parameters: phaseRangeOption ( NXOpen.CAE.Xyplot.PhaseRangeOption
) – Phase range optionNew in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)