DecimalFormat Enumeration¶
-
class
NXOpen.CAE.Xyplot.
DecimalFormat
¶ Bases:
object
Represents the decimal number format Enum Members
- for example: 5.3E+05 “
- “Xxexx”, ” Scientific notation with two digits followed by period ” “Xxxexx”, ” Scientific notation with three digits followed by period ” “Xxxxexx”, ” Scientific notation with four digits followed by period “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.