BasicModel Class¶
-
class
NXOpen.CAE.Xyplot.
BasicModel
¶ Bases:
NXOpen.TaggedObject
Represents a abstract component object on a XY graphing.
Not support KF.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DisplayStyle | Returns the model display style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Find | Finds the NXObject with the given identifier as recorded in a journal. |
Property Detail¶
DisplayStyle¶
-
BasicModel.
DisplayStyle
¶ Returns the model display style
-------------------------------------
Getter Method
Signature
DisplayStyle()
Returns: Model display style Return type: NXOpen.CAE.Xyplot.IDisplayStyle
New in version NX10.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
Method Detail¶
Find¶
-
BasicModel.
Find
¶ Finds the
NXObject
with the given identifier as recorded in a journal. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX10.0.0.
License requirements: None.