VelocityImpactDirection Class¶
-
class
NXOpen.CAE.ResponseSimulation.
VelocityImpactDirection
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.CAE.ResponseSimulation.VelocityImpactDirection
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DirectionOption | Returns or sets the direction option |
NodalComponent | Returns or sets the selected nodal component |
ReverseDirection | Returns or sets the option to reverse direction of nodal component or not. |
Tag | Returns the Tag for this object. |
UserDefinedDirection | Returns or sets the user-defined direction |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
VelocityImpactDirectionDirectionType Enumeration | the direction options for impact |
VelocityImpactDirectionNodalComponentType Enumeration | the types of nodal component |
Property Detail¶
DirectionOption¶
-
VelocityImpactDirection.
DirectionOption
¶ Returns or sets the direction option
-------------------------------------
Getter Method
Signature
DirectionOption()
Returns: Return type: NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionOption(mDirectionOption)
Parameters: mDirectionOption ( NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
NodalComponent¶
-
VelocityImpactDirection.
NodalComponent
¶ Returns or sets the selected nodal component
-------------------------------------
Getter Method
Signature
NodalComponent()
Returns: Return type: NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NodalComponent(nodalComponent)
Parameters: nodalComponent ( NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionNodalComponentType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ReverseDirection¶
-
VelocityImpactDirection.
ReverseDirection
¶ Returns or sets the option to reverse direction of nodal component or not.
Only valid when direction option is
NXOpen.CAE.ResponseSimulation.VelocityImpactDirectionDirectionType.NodalComponent
-------------------------------------
Getter Method
Signature
ReverseDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection(reverseDirection)
Parameters: reverseDirection (bool) – New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
UserDefinedDirection¶
-
VelocityImpactDirection.
UserDefinedDirection
¶ Returns or sets the user-defined direction
-------------------------------------
Getter Method
Signature
UserDefinedDirection()
Returns: Return type: NXOpen.Direction
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserDefinedDirection(userDefinedDirection)
Parameters: userDefinedDirection ( NXOpen.Direction
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
VelocityImpactDirection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.