RotationalNodalFunctionExcitationBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
RotationalNodalFunctionExcitationBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.NodalFunctionExcitationBuilder
Represents the manager to
NXOpen.CAE.ResponseSimulation.RotationalNodalFunctionExcitation
.The objects of
NXOpen.CAE.ResponseSimulation.RotationalNodalFunctionExcitation
can be created or edited on through this class To create a new instance of this class, useNXOpen.CAE.ResponseSimulation.ExcitationCollection.CreateRotationalNodalFunctionExcitationBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DynamicEvent | Returns the parent dynamic event object |
ExcitationLocationDefinition | Returns the excitation location definition |
FunctionComponentRx | Returns the function component of Rx direction |
FunctionComponentRy | Returns the function component of Ry direction |
FunctionComponentRz | Returns the function component of Rz direction |
ObjectLabel | Returns the object label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FunctionComponentRx¶
-
RotationalNodalFunctionExcitationBuilder.
FunctionComponentRx
¶ Returns the function component of Rx direction
-------------------------------------
Getter Method
Signature
FunctionComponentRx()
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FunctionComponentRy¶
-
RotationalNodalFunctionExcitationBuilder.
FunctionComponentRy
¶ Returns the function component of Ry direction
-------------------------------------
Getter Method
Signature
FunctionComponentRy()
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
FunctionComponentRz¶
-
RotationalNodalFunctionExcitationBuilder.
FunctionComponentRz
¶ Returns the function component of Rz direction
-------------------------------------
Getter Method
Signature
FunctionComponentRz()
Returns: Return type: NXOpen.CAE.ResponseSimulation.FunctionComponentData
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
RotationalNodalFunctionExcitationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.