NodalFunctionEvalBeamLocation Enumeration¶
-
class
NXOpen.CAE.ResponseSimulation.
NodalFunctionEvalBeamLocation
¶ Bases:
object
Specifies beam element evaluation locations for nodal function evaluation Enum Members
Enum Member Enum Member Description C Stress Recovery point C on a beam cross sectionD Stress Recovery point D on a beam cross sectionE Stress Recovery point E on a beam cross sectionF Stress Recovery point F on a beam cross sectionAll All four Stress Recovery points on a beam cross section-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-