ElementalFunctionEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
ElementalFunctionEvaluationSettingBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.FunctionEvaluationSettingBuilder
This is a manager to the
NXOpen.CAE.ResponseSimulation.ElementalFunctionEvaluationSetting
class.Object of type
NXOpen.CAE.ResponseSimulation.ElementalFunctionEvaluationSetting
can be created and edited only through this classTo create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.EvaluationSettingManager.CreateElementalFunctionEvaluationSettingBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BeamDataLocation | Returns or sets the data location of beam element. |
CoordinateSystem | Returns or sets the coordinate system |
DataComponent | Returns or sets the data component of direction |
ElementLocation | Returns or sets the evaluation location of element. |
OutputSettings | Returns the output setting. |
ResultType | Returns or sets the result type |
ShellEvaluationLocation | Returns or sets the evaluation location of shell element. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDestinationElements | Returns the destination elements @return |
GetObject | Returns the object currently being edited by this builder. |
SetDestinationElements | Sets the destination elements |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BeamDataLocation¶
-
ElementalFunctionEvaluationSettingBuilder.
BeamDataLocation
¶ Returns or sets the data location of beam element.
For more information about beam data location, see the Response Simulatin section of the Gateway help
-------------------------------------
Getter Method
Signature
BeamDataLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ElementalFunctionEvalBeamLocation
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
BeamDataLocation(beamLocation)
Parameters: beamLocation ( NXOpen.CAE.ResponseSimulation.ElementalFunctionEvalBeamLocation
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
CoordinateSystem¶
-
ElementalFunctionEvaluationSettingBuilder.
CoordinateSystem
¶ Returns or sets the coordinate system
-------------------------------------
Getter Method
Signature
CoordinateSystem()
Returns: Return type: NXOpen.CAE.ResponseSimulation.CoordinateSystem
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
CoordinateSystem(coordinateSystem)
Parameters: coordinateSystem ( NXOpen.CAE.ResponseSimulation.CoordinateSystem
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
DataComponent¶
-
ElementalFunctionEvaluationSettingBuilder.
DataComponent
¶ Returns or sets the data component of direction
-------------------------------------
Getter Method
Signature
DataComponent()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DirectionDataComponent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
DataComponent(dataComponent)
Parameters: dataComponent ( NXOpen.CAE.ResponseSimulation.DirectionDataComponent
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ElementLocation¶
-
ElementalFunctionEvaluationSettingBuilder.
ElementLocation
¶ Returns or sets the evaluation location of element.
-------------------------------------
Getter Method
Signature
ElementLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ElementLocation
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ElementLocation(elementLocation)
Parameters: elementLocation ( NXOpen.CAE.ResponseSimulation.ElementLocation
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ShellEvaluationLocation¶
-
ElementalFunctionEvaluationSettingBuilder.
ShellEvaluationLocation
¶ Returns or sets the evaluation location of shell element.
-------------------------------------
Getter Method
Signature
ShellEvaluationLocation()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ShellElementEvaluationLocation
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ShellEvaluationLocation(shellLocation)
Parameters: shellLocation ( NXOpen.CAE.ResponseSimulation.ShellElementEvaluationLocation
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetDestinationElements¶
-
ElementalFunctionEvaluationSettingBuilder.
GetDestinationElements
¶ Returns the destination elements
Signature
GetDestinationElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDestinationElements¶
-
ElementalFunctionEvaluationSettingBuilder.
SetDestinationElements
¶ Sets the destination elements
Signature
SetDestinationElements(destinationElement)
Parameters: destinationElement (list of NXOpen.CAE.FEElement
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
ElementalFunctionEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.