DDAMComponentData Class¶
-
class
NXOpen.CAE.ResponseSimulation.
DDAMComponentData
¶ Bases:
NXOpen.TaggedObject
Represents an excitation on one specified direction.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
LoadingTypeOption | Returns or sets the option of loading type |
ResponseTypeOption | Returns or sets the option of response type |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetComponentType | Returns the component type @return |
GetEnable | Returns the enable option @return |
Enumerations¶
DDAMComponentDataLoadingType Enumeration | Specifies the loading type |
DDAMComponentDataResponseType Enumeration | Specifies the response type |
Property Detail¶
LoadingTypeOption¶
-
DDAMComponentData.
LoadingTypeOption
¶ Returns or sets the option of loading type
-------------------------------------
Getter Method
Signature
LoadingTypeOption()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DDAMComponentDataLoadingType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
LoadingTypeOption(loadingType)
Parameters: loadingType ( NXOpen.CAE.ResponseSimulation.DDAMComponentDataLoadingType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ResponseTypeOption¶
-
DDAMComponentData.
ResponseTypeOption
¶ Returns or sets the option of response type
-------------------------------------
Getter Method
Signature
ResponseTypeOption()
Returns: Return type: NXOpen.CAE.ResponseSimulation.DDAMComponentDataResponseType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ResponseTypeOption(responseType)
Parameters: responseType ( NXOpen.CAE.ResponseSimulation.DDAMComponentDataResponseType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetComponentType¶
-
DDAMComponentData.
GetComponentType
¶ Returns the component type
Signature
GetComponentType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ExcitationComponent
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)