CSDExcitationBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
CSDExcitationBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.ExcitationBuilder
Represents the manager to
NXOpen.CAE.ResponseSimulation.CSDExcitation
.The object of type
NXOpen.CAE.ResponseSimulation.CSDExcitation
can only be created or edited through this class.To create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.ExcitationCollection.CreateCsdExcitationBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CorrelationType | Returns or sets the correlation type |
CorrelationValue | Returns or sets the correlation type |
DynamicEvent | Returns the parent dynamic event object |
ExcitationLocationDefinition | Returns the excitation location definition |
ObjectLabel | Returns the object label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFromFunction | Returns the from function @return |
GetObject | Returns the object currently being edited by this builder. |
GetToFunction | Returns the to function @return |
SetFromFunction | Sets the from function |
SetToFunction | Sets the to function |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CorrelationType¶
-
CSDExcitationBuilder.
CorrelationType
¶ Returns or sets the correlation type
-------------------------------------
Getter Method
Signature
CorrelationType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.CSDExcitationCorrelationType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
CorrelationType(type)
Parameters: type ( NXOpen.CAE.ResponseSimulation.CSDExcitationCorrelationType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
CorrelationValue¶
-
CSDExcitationBuilder.
CorrelationValue
¶ Returns or sets the correlation type
-------------------------------------
Getter Method
Signature
CorrelationValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
CorrelationValue(correlationValue)
Parameters: correlationValue (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetFromFunction¶
-
CSDExcitationBuilder.
GetFromFunction
¶ Returns the from function
Signature
GetFromFunction()
Returns: a tuple Return type: A tuple consisting of (fromExcitation, componentType). fromExcitation is a NXOpen.CAE.ResponseSimulation.Excitation
. componentType is aNXOpen.CAE.ResponseSimulation.ExcitationComponent
.New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetToFunction¶
-
CSDExcitationBuilder.
GetToFunction
¶ Returns the to function
Signature
GetToFunction()
Returns: a tuple Return type: A tuple consisting of (toExcitation, componentType). toExcitation is a NXOpen.CAE.ResponseSimulation.Excitation
. componentType is aNXOpen.CAE.ResponseSimulation.ExcitationComponent
.New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetFromFunction¶
-
CSDExcitationBuilder.
SetFromFunction
¶ Sets the from function
Signature
SetFromFunction(fromExcitation, componentType)
Parameters: - fromExcitation (
NXOpen.CAE.ResponseSimulation.Excitation
) – - componentType (
NXOpen.CAE.ResponseSimulation.ExcitationComponent
) –
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
- fromExcitation (
SetToFunction¶
-
CSDExcitationBuilder.
SetToFunction
¶ Sets the to function
Signature
SetToFunction(toExcitation, componentType)
Parameters: - toExcitation (
NXOpen.CAE.ResponseSimulation.Excitation
) – - componentType (
NXOpen.CAE.ResponseSimulation.ExcitationComponent
) –
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
- toExcitation (
Validate¶
-
CSDExcitationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.