TBSShapeOptimizationSolution Class¶
-
class
NXOpen.CAE.Optimization.
TBSShapeOptimizationSolution
¶ Bases:
NXOpen.CAE.Optimization.TBSOptimizationSolution
,NXOpen.CAE.Optimization.TBSIOptimizationTest
Represents a shape optimization solution
To create or edit an instance of this class, use
NXOpen.CAE.Optimization.TBSShapeOptimizationSolutionBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ControlParameters | Returns the parameters to control optimization |
DesignArea | Returns the design area that will be modified during optimization |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MeshSmooth | Returns the mesh smooth definition |
Name | Returns the custom name of the object. |
Objectives | Returns the objective function of the optimization |
OutputControlOptions | Returns the output control options of the optimization |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StopCondition | Returns the stop condition to end the optimization |
Tag | Returns the Tag for this object. |
TestFunction | Returns the test function |
Methods¶
Method | Description |
---|---|
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
Destroy | Deletes an optimization solution and the associated result file optional |
Find | Finds the NXOpen.TaggedObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetIterationNumber | Returns the iteration number during the optimization @return |
GetPostResult | Returns the post result file name and status @return |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSmoothResult | Returns the result file name and status for a specified smoothing setting @return |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTestResultFile | Returns the file name of test result @return |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
Prints a representation of this object to the system log file. | |
Rename | Rename Solution and optionally rename associated results files |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Solve | Solves the optimization solution |
SolveTest | Solves optimization test |
Property Detail¶
IsOccurrence¶
-
TBSShapeOptimizationSolution.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
TBSShapeOptimizationSolution.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MeshSmooth¶
-
TBSShapeOptimizationSolution.
MeshSmooth
¶ Returns the mesh smooth definition
-------------------------------------
Getter Method
Signature
MeshSmooth()
Returns: Return type: NXOpen.CAE.Optimization.TBSMeshSmooth
New in version NX8.5.0.
License requirements: None.
Name¶
-
TBSShapeOptimizationSolution.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
TBSShapeOptimizationSolution.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
TBSShapeOptimizationSolution.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
TBSShapeOptimizationSolution.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
TestFunction¶
-
TBSShapeOptimizationSolution.
TestFunction
¶ Returns the test function
-------------------------------------
Getter Method
Signature
TestFunction()
Returns: Return type: NXOpen.CAE.Optimization.TBSTestFunction
New in version NX8.5.0.
License requirements: None.
Method Detail¶
FindObject¶
-
TBSShapeOptimizationSolution.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetTestResultFile¶
-
TBSShapeOptimizationSolution.
GetTestResultFile
¶ Returns the file name of test result
Signature
GetTestResultFile()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
Print¶
-
TBSShapeOptimizationSolution.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
TBSShapeOptimizationSolution.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.