TBSCheckDOFDofSettings_Struct Struct¶
NXOpen.CAE.Optimization.TBSCheckDOF.DofSettings is an alias for NXOpen.CAE.Optimization.TBSCheckDOFDofSettings_Struct
-
class
NXOpen.CAE.Optimization.
TBSCheckDOFDofSettings_Struct
¶ Bases:
object
the displacement restriction settings on three axial directions of referenced coordinate system
Fields¶
Field | Description |
---|---|
Dof1 | Represents displacement in the X axial direction |
Dof2 | Represents displacement in the Y axial direction |
Dof3 | Represents displacement in the Z axial direction |
Dof1¶
-
TBSCheckDOFDofSettings_Struct.
Dof1
¶ Represents displacement in the X axial direction
-------------------------------------
Getter Method Signature
Dof1()
Returns: Return type: NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
-------------------------------------
Setter Method
Signature
Dof1(value)
Parameters: value ( NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
) –
Dof2¶
-
TBSCheckDOFDofSettings_Struct.
Dof2
¶ Represents displacement in the Y axial direction
-------------------------------------
Getter Method Signature
Dof2()
Returns: Return type: NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
-------------------------------------
Setter Method
Signature
Dof2(value)
Parameters: value ( NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
) –
Dof3¶
-
TBSCheckDOFDofSettings_Struct.
Dof3
¶ Represents displacement in the Z axial direction
-------------------------------------
Getter Method Signature
Dof3()
Returns: Return type: NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
-------------------------------------
Setter Method
Signature
Dof3(value)
Parameters: value ( NXOpen.CAE.Optimization.TBSCheckDOFCheckDofOption
) –