TBSCastConditionMiddlePlaneType Enumeration¶
NXOpen.CAE.Optimization.TBSCastCondition.MiddlePlaneType is an alias for NXOpen.CAE.Optimization.TBSCastConditionMiddlePlaneType
-
class
NXOpen.CAE.Optimization.
TBSCastConditionMiddlePlaneType
¶ Bases:
object
Defines the middle plane type
Enum Members
Enum Member Enum Member Description None No definition of a central planeAutomatic Automatica determinaton of the central planeAutomaticTight No holes are generated in the central planePoint A point within the central plane from which the deformation vector is positioned perpendicular toSurface The elements are demolded at the actual surface of the restrict areaStamp The element group is demolded keeping a stampable structure-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-