DataManagerAfuRecordZValue Enumeration¶
NXOpen.CAE.FTK.DataManager.AfuRecordZValue is an alias for NXOpen.CAE.FTK.DataManagerAfuRecordZValue
-
class
NXOpen.CAE.FTK.
DataManagerAfuRecordZValue
¶ Bases:
object
Represents the method to get Z value for afu record in 3D plot
Enum Members
Enum Member Enum Member Description SelectionOrder The Z value is selection orderGeneral The Z value is attribute of General field in an afu recordRpm The z value is attribute of RPM field in an afu recordTime The z value is attribute of Time field in an afu recordOrder The z value is attribute of Order field in an afu record-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-