OnestepUnformBuilderDisplaySpringbackMode Enumeration¶
NXOpen.BodyDes.OnestepUnformBuilder.DisplaySpringbackMode is an alias for NXOpen.BodyDes.OnestepUnformBuilderDisplaySpringbackMode
-
class
NXOpen.BodyDes.
OnestepUnformBuilderDisplaySpringbackMode
¶ Bases:
object
The mode of display springback.
Enum Members
Enum Member Enum Member Description Displacement Onestep display springback mode is displacement Alongx Onestep display springback mode is along X Alongy Onestep display springback mode is along Y Alongz Onestep display springback mode is along Z -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-