OnestepUnformBuilderConvergency Enumeration¶
NXOpen.BodyDes.OnestepUnformBuilder.Convergency is an alias for NXOpen.BodyDes.OnestepUnformBuilderConvergency
-
class
NXOpen.BodyDes.
OnestepUnformBuilderConvergency
¶ Bases:
object
The solver convergency level of onestep unform.
Enum Members
Enum Member Enum Member Description Low Onestep solver convergency level is low Medium Onestep solver convergency level is medium High Onestep solver convergency level is high -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-