SelectObjectFilterType Enumeration

NXOpen.BlockStyler.SelectObject.FilterType is an alias for NXOpen.BlockStyler.SelectObjectFilterType

class NXOpen.BlockStyler.SelectObjectFilterType

Bases: object

Indicates the general filter type for selection.

Enum Members

Enum Member Enum Member Description
Features
Filter to select all feature types
Faces
Filter to select all face types
Edges
Filter to select all edge types
CurvesAndEdges
Filter to select all curve and edge types
Components
Filter to select all components
SolidBodies
Filter to select all solid bodies
SheetBodies
Filter to select all sheet bodies
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.