ReverseDirection Class¶
-
class
NXOpen.BlockStyler.
ReverseDirection
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents Reverse Direction block
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Direction | Returns or sets the Direction. |
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Flip | Returns or sets the Flip. |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
Name | Returns the name of the block or BlockID |
Origin | Returns or sets the Origin. |
Show | Returns or sets the Visibility of block. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetProperties | Returns the properties of the block @return |
Property Detail¶
Direction¶
-
ReverseDirection.
Direction
¶ Returns or sets the Direction.
It specifies the orientation of direction handle.
-------------------------------------
Getter Method
Signature
Direction()
Returns: Return type: NXOpen.Vector3d
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Direction(direction)
Parameters: direction ( NXOpen.Vector3d
) –New in version NX8.5.0.
License requirements: None.
Flip¶
-
ReverseDirection.
Flip
¶ Returns or sets the Flip.
If true, the handle is flipped opposite of the direction.
-------------------------------------
Getter Method
Signature
Flip()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Flip(flip)
Parameters: flip (bool) – New in version NX8.5.0.
License requirements: None.
Origin¶
-
ReverseDirection.
Origin
¶ Returns or sets the Origin.
It specifies the origin of direction handle.
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Point3d
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Origin(origin)
Parameters: origin ( NXOpen.Point3d
) –New in version NX8.5.0.
License requirements: None.