PropertyListPropertyType Enumeration

NXOpen.BlockStyler.PropertyList.PropertyType is an alias for NXOpen.BlockStyler.PropertyListPropertyType

class NXOpen.BlockStyler.PropertyListPropertyType

Bases: object

Represents the property types.

Enum Members

Enum Member Enum Member Description
String String
Double Double
Logical Logical
Integer Integer
Enum Enum
Strings Strings
UIBlock UIBlock
Point Point
Vector Vector
Bits Bits
TaggedObject Tagged Object
Array Array
IntegerMatrix2d Integer 2d-Matrix
DoubleMatrix2d Double 2d-Matrix
TaggedObjectMatrix2d Tagged Object 2d-Matrix
IntegerVector Integer Vector
DoubleVector Double Vector
TaggedObjectVector Tagged Object Vector
File File
SelectionFilter Selection Filter
Undefined Undefined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.