PropertyListListMode Enumeration

NXOpen.BlockStyler.PropertyList.ListMode is an alias for NXOpen.BlockStyler.PropertyListListMode

class NXOpen.BlockStyler.PropertyListListMode

Bases: object

Indicates whether the properties in the list are named.

Enum Members

must be indexed through an integer index “
“Named”, ” The properties are named “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.