NodeDropType Enumeration¶
NXOpen.BlockStyler.Node.DropType is an alias for NXOpen.BlockStyler.NodeDropType
-
class
NXOpen.BlockStyler.
NodeDropType
¶ Bases:
object
Represents the drop type
Enum Members
Enum Member Enum Member Description None Drop not permitted On Drop permitted on the target node Before Drop permitted before the target node After Drop permitted after the target node BeforeAndAfter Drop permitted before and after the target node -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-