LineWidth Class¶
-
class
NXOpen.BlockStyler.
LineWidth
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents a Line Width block
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AllowDefaultWidth | Returns the AllowDefaultWidth |
AllowNoChangeWidth | Returns the AllowNoChangeWidth. |
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
LabelVisibility | Returns or sets the LabelVisibility |
LineWidthValue | Returns or sets the LineWidthValue |
Name | Returns the name of the block or BlockID |
Show | Returns or sets the Visibility of block. |
ShowDefaultAsOriginal | Returns the ShowDefaultAsOriginal. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetProperties | Returns the properties of the block @return |
Property Detail¶
AllowDefaultWidth¶
-
LineWidth.
AllowDefaultWidth
¶ Returns the AllowDefaultWidth
-------------------------------------
Getter Method
Signature
AllowDefaultWidth()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
AllowNoChangeWidth¶
-
LineWidth.
AllowNoChangeWidth
¶ Returns the AllowNoChangeWidth.
If true, no change in width is allowed.
-------------------------------------
Getter Method
Signature
AllowNoChangeWidth()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
LabelVisibility¶
-
LineWidth.
LabelVisibility
¶ Returns or sets the LabelVisibility
-------------------------------------
Getter Method
Signature
LabelVisibility()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LabelVisibility(visible)
Parameters: visible (bool) – New in version NX8.5.0.
License requirements: None.
LineWidthValue¶
-
LineWidth.
LineWidthValue
¶ Returns or sets the LineWidthValue
-------------------------------------
Getter Method
Signature
LineWidthValue()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineWidthValue(widthValue)
Parameters: widthValue (int) – New in version NX8.5.0.
License requirements: None.