LineFont Class¶
-
class
NXOpen.BlockStyler.
LineFont
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents a Line Width block
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AvailableOptions | Returns or sets the Available Options |
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
Name | Returns the name of the block or BlockID |
Show | Returns or sets the Visibility of block. |
ShowOptionLabels | Returns or sets the show option labels |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
ValueAsString | Returns or sets the value |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetProperties | Returns the properties of the block @return |
Property Detail¶
AvailableOptions¶
-
LineFont.
AvailableOptions
¶ Returns or sets the Available Options
-------------------------------------
Getter Method
Signature
AvailableOptions()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AvailableOptions(availableOptions)
Parameters: availableOptions (int) – New in version NX9.0.0.
License requirements: None.
ShowOptionLabels¶
-
LineFont.
ShowOptionLabels
¶ Returns or sets the show option labels
-------------------------------------
Getter Method
Signature
ShowOptionLabels()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowOptionLabels(showOptionLabels)
Parameters: showOptionLabels (bool) – New in version NX9.0.0.
License requirements: None.
ValueAsString¶
-
LineFont.
ValueAsString
¶ Returns or sets the value
-------------------------------------
Getter Method
Signature
ValueAsString()
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValueAsString(fontValueString)
Parameters: fontValueString (str) – New in version NX9.0.0.
License requirements: None.